MSP430 GCC supports Windows, Linux, and
macOS:
- Windows 7 32 bit or 64 bit
- Windows 8 32 bit or 64 bit
- Windows 10 32 bit or 64 bit
- Linux 32 bit or 64 bit
- macOS 64 bit
You can install the MSP430 GCC using any of
the following methods:
- MSP430 GCC toolchain is installed by
default by CCS v7.2 and higher.
- In CCS releases prior to v7.2, the MSP430 GCC (toolchain only) is
available in the CCS Apps Center. The corresponding MSP430 GCC support files (header and
linkers) are downloaded with a standard MSP430 emulation package. For details, see Section 2.1.
- MSP430 GCC can be also downloaded as stand-alone package. For details, see Section 2.2.