SLAU678C March 2016 – November 2022
The MSP-EXP430FR5994 provides external clocks in addition to the internal clocks in the device.
The 32-kHz crystal allows for lower LPM3 sleep currents than do the other low-frequency clock sources. Therefore, the presence of the crystal allows the full range of low-power modes to be used.
The high-frequency crystal is not populated by default, but the footprint for a crystal is provided. Populate a high-frequency crystal for applications that need more precise high-frequency clock sources than the internal DCO.
The internal clocks in the device default to the following configuration:
For more information about configuring internal clocks and using the external oscillators, see the MSP430FR58xx, MSP430FR59xx, and MSP430FR6xx Family User's Guide.