SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
For image sources that are 8 bpp, 256 palette entries (28) are required. This structure of the palette RAM is similar to the one described for 1, 2, 4, or 4 bpp except that the palette requires 256 entries (128 words), instead of 16. The first palette entry again contains the "type" definition of the picture along with the RGB values in bits [11:0].