SLAU723A October 2017 – October 2018 MSP432E401Y , MSP432E411Y
Analog-to-Digital Converter Peripheral Ready (PRADC)
The PRADC register indicates whether the ADC modules are ready to be accessed by software following a change in status of power, run mode clocking, or reset. A power change is initiated if the corresponding PCADC bit is changed from 0 to 1. A run mode clocking change is initiated if the corresponding RCGCADC bit is changed. A reset change is initiated if the corresponding SRADC bit is changed from 0 to 1.
The PRADC bit is cleared on any of the preceding events and is not set again until the module is completely powered, enabled, and internally reset.
PRADC is shown in Figure 4-187 and described in Table 4-215.
Return to Summary Table.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||||||||||
R-0x0 | |||||||||||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | R1 | R0 | |||||||||||||
R-0x0 | R-0x0 | R-0x0 | |||||||||||||