15.4.2.7.4 Read from Extended PHY Registers
The following describes the steps to read from an extended PHY register.
- Check the MIIB bit in the EMACMIIADDR register to identify if the MII interface is busy. When the MIIB bit is 0, the MII interface is available to read to the PHY registers.
- Initiate the read by writing the EMACMIIADDR register fields:
- PLA: Physical Layer Address of the PHY. The integrated PHY's address is 0x0. The values 0x1 to 0x1F are available for external PHYs.
- MII: Register address of PHY register to be written.
- CR: Clock Reference for the MDIO interface.
- MIIW: Write/Read Initiation. This bit is programmed to a 0 to indicate that a read operation is to be executed.
- MIIB: MII Busy. This bit is set to 1 to indicate that the MII is now busy with a read operation. The EMAC clears this bit when the write has been transmitted.
- Wait for the write to complete by polling the MIIB bit.
- When the MIIB is clear, read the contents of the EMACMIIDATA register.