SLAU739 October   2017

 

  1.   MSP430FR2433 LaunchPad™ Development Kit (MSP‑EXP430FR2433)
    1.     Trademarks
    2. 1 Getting Started
      1. 1.1 Introduction
      2. 1.2 Key Features
      3. 1.3 What's Included
        1. 1.3.1 Kit Contents
        2. 1.3.2 Software Examples
      4. 1.4 First Steps: Out-of-Box Experience
        1. 1.4.1 Connecting to the Computer
        2. 1.4.2 Running the Out-of-Box Demo
      5. 1.5 Next Steps: Looking Into the Provided Code
    3. 2 Hardware
      1. 2.1 Block Diagram
      2. 2.2 Hardware Features
        1. 2.2.1 MSP430FR2433 MCU
        2. 2.2.2 eZ-FET Onboard Debug Probe With EnergyTrace Technology
        3. 2.2.3 Debug Probe Connection: Isolation Jumper Block
        4. 2.2.4 Application (or Backchannel) UART
        5. 2.2.5 Optional Features
          1. 2.2.5.1 Supercapacitor
      3. 2.3 Power
        1. 2.3.1 eZ-FET USB Power
        2. 2.3.2 BoosterPack and External Power Supply
        3. 2.3.3 Supercap (C6)
          1. 2.3.3.1 Charging the Supercap
          2. 2.3.3.2 Using the Supercap
          3. 2.3.3.3 Disabling the Supercap
      4. 2.4 Measure Current Draw of the MSP430 MCU
      5. 2.5 Clocking
      6. 2.6 Using the eZ-FET Debug Probe With a Different Target
      7. 2.7 BoosterPack Pinout
      8. 2.8 Design Files
        1. 2.8.1 Hardware
        2. 2.8.2 Software
      9. 2.9 Hardware Change log
    4. 3 Software Examples
      1. 3.1 Out-of-Box Software Example
        1. 3.1.1 Source File Structure
        2. 3.1.2 Overview
        3. 3.1.3 FRAM Data Logging Mode
        4. 3.1.4 Live Temperature Mode
      2. 3.2 Blink LED Example
        1. 3.2.1 Source File Structure
    5. 4 Resources
      1. 4.1 Integrated Development Environments
        1. 4.1.1 TI Cloud Development Tools
          1. 4.1.1.1 TI Resource Explorer Cloud
          2. 4.1.1.2 Code Composer Studio Cloud
        2. 4.1.2 Code Composer Studio IDE
        3. 4.1.3 IAR Embedded Workbench for Texas Instruments 430
      2. 4.2 LaunchPad Websites
      3. 4.3 MSPWare and TI Resource Explorer
      4. 4.4 FRAM Utilities
        1. 4.4.1 Compute Through Power Loss (CTPL)
        2. 4.4.2 Nonvolatile Storage (NVS)
      5. 4.5 MSP430FR2433 MCU
        1. 4.5.1 Device Documentation
        2. 4.5.2 MSP430FR2433 Code Examples
        3. 4.5.3 MSP430 Application Notes and TI Designs
      6. 4.6 Community Resources
        1. 4.6.1 TI E2E Community
        2. 4.6.2 Community at Large
    6. 5 FAQ
    7. 6 Schematics

Using the eZ-FET Debug Probe With a Different Target

The eZ-FET debug probe on the LaunchPad can interface to most MSP430 derivative devices, not just the onboard MSP430FR2433 target device.

To do this, disconnect every jumper in the isolation jumper block. This is necessary, because the debug probe cannot connect to more than one target at a time over the Spy-Bi-Wire (SBW) connection.

Next, make sure the target board has proper connections for SBW. To be compatible with SBW, the capacitor on RST/SBWTDIO cannot be greater than 2.2 nF. The documentation for designing MSP430 JTAG interface circuitry is the MSP430 Hardware Tools User's Guide.

Finally, wire together these signals from the debug probe side of the isolation jumper block to the target hardware:

  • 5 V (if 5 V is needed)
  • 3.3 V
  • GND
  • SBWTDIO
  • SBWTCK
  • TXD (if the UART backchannel is to be used)
  • RXD (if the UART backchannel is to be used)

This wiring can be done either with jumper wires or by designing the board with a connector that plugs into the isolation jumper block.