SLAU748B October 2017 – September 2018 MSP432E401Y
The Ethernet LaunchPad development kit comes with an onboard XDS-110. The XDS-110 allows for the programming and debugging of the MSP432E401Y using Code Composer Studio™ IDE or any of the supported tool chains. Note that XDS-110 only supports JTAG debugging at this time.
Debugging external boards using the XDS-110 is possible by removing the TDI, TDO, TCK, TMS, and RST jumpers from JP101 on the Ethernet LaunchPad development kit and using the XDS-110 to drive JTAG signals out on J102. To restore the connection to the onboard MSP432E401Y microcontroller, reinstall the jumpers on JP101.