SLAU776A May 2018 – December 2023 ADC12DL2500 , ADC12DL3200
This appendix provides settings for modifying the EVM for optional clocking support.
The LMK04828 provides a buffered copy of the onboard 100-MHz VCXO to the LMX2582. When the optional 10-MHz reference clock is connected, the 100-MHz VCXO output is frequency locked to the 10-MHz reference. This process enables coherent sampling of the analog input signal. The EVM can be configured to use an external ADC clock with the following steps (see Figure 6-1):
The ADC12DL3200EVM includes a reference clock input (CLKIN0) that allows the user to sync the LMK04828 to an external 10-MHz reference allowing for coherent sampling
The LMX2582 and LMK04828 may be reconfigured to exercise more features, but this EVM is not intended to be a full evaluation platform for these devices. For a full evaluation platform, see the LMK04828 tool folder and LMX2582 tool folder.