SLAU789A November 2023 – November 2023
Control of the TSW1418EVM is through USB connector J2. This connector provides the interface between HSDC Pro GUI running on a PC using the Windows® operating system and the FPGA. For the computer, the drivers needed to access the USB port are included on the HSDC Pro GUI installation software that can be downloaded from the Texas Instruments website. The drivers are automatically installed during the installation process. On the TSW1418EVM, the USB port is used to power up the EVM, identify the type and serial number of the EVM under test, load the desired FPGA configuration file, and capture data from ADC EVMs.