SLAU789A November 2023 – November 2023
One LED on the TSW1418EVM is used to indicate the presence of power on the board. The description of this LED can be found in Table 3-3.
Component | Description |
---|---|
D2 | If this is on, then that indicates the presence of 5 V on the board. |