SLAU802 March 2019
The eZ-FET debug probe on the LaunchPad development kit can interface to most MSP430 MCUs, not just the onboard MSP430FR2476 target device.
To interface to another MCU, disconnect all jumpers in the isolation jumper block. This is necessary because the debug probe cannot connect to more than one target at a time over the Spy-Bi-Wire (SBW) connection.
Next, make sure the target board has proper connections for SBW. To be compatible with SBW, the capacitor on RST/SBWTDIO must be 2.2 nF or less. For documentation on designing MSP430 JTAG interface circuitry, see the MSP430 Hardware Tools User's Guide.
Finally, wire together the following signals from the debug probe side of the isolation jumper block to the target hardware:
This wiring can be done either with jumper wires or by designing the board with a connector that plugs into the isolation jumper block.