UltraScale is a trademark of Xilinx Incorporated.
Xilinx, AlphaData ADA-SDEV-KIT1&2, Vivado, space grade Xilinx, Kintex, are registered trademarks of Xilinx Incorporated.
Microsoft and Windows are registered trademarks of Microsoft Corporation.
All other trademarks are the property of their respective owners.
This design is developed for the Alpha Data System Development Kit (SDEV) to interface with the ADC12DJ3200EVMCVAL using JMODE0. This design uses custom TI JESD204B IP, which implements both JESD204B Base IP and JESD204B PHY IP to get JESD204B data from the ADC12DJ3200QML-SP device at 6.2 GSPS in single-device mode with 12.4 Gbps data lane rate. The reference design implements a transport layer that collects 40 samples from the 8 lanes (as depicted in the JMODE0 table of the data sheet). The samples are captured using the Xilinx Internal Logic Analyzer (ILA) tool and offloaded to a PC were the results can be displayed using the TI High-Speed Data Converter Pro GUI.
The AlphaData SDEV has a standard FMC+ connector that provides an interface between this board and the TI JESD204B ADC12DJ3200CEVMCVAL. For communicating, the AlphaData SDEV uses JTAG to acquire and receive data using a host PC. The industry-standard JTAG connector is used for configuring the FPGA using the Vivado® Design Suite, a design tool by Xilinx. The firmware designed for this integration only supports JMODE0 at 6.2 GSPS single ADC. Future firmware will support all modes of this ADC.
The ADA-SDEV-KIT1&2 includes the ADM-SDEV-BASE/XCKU060-AD01360 Evaluation board which contains a Xilinx XQRKU060-CNA1509 FPGA and the ADM-SDEV-CFG1-AD01361 USB interface board. For more information regarding these boards, see the AlphaData website.