The following instructions describe
how to set up and use the EVM.
- Download this driver and install it as an administrator: https://www.ti.com/lit/zip/sbac253.
- Follow the download prompts, a myTI account will be required.
- Note that this driver is labeled as a PAMB driver, but is also used for
the SCB.
- Attach a compatible EVM to the SCB
Controller, such as the one in Figure 3-1.
- Connect the EVM to the PC using the
provided USB cable.
- Insert the micro USB cable
into the SCB Controller onboard USB receptacle J2.
- Plug the other end of the
USB cable into a PC.
- Launch the appropriate EVM GUI, per instructions from the EVM specific
user's guide in either Chrome, Firefox, or Safari.
- Connect the GUI to the SCB, and update the firmware.
- Press the connect symbol in the bottom left corner.
- Go to File -> Program Device...
- For more details see Section 3.2.2.1.
- Use the EVM/SCB as described in the EVM-specific user's guide.