SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519
When using a capture/compare pin (CCP) as an input, configure the pin control management register (PINCMx) for the TIMx CCP input. Refer to the device data sheet for TIMx CCP pinmux input options, such as TIMG0_C0.
The CCP input signal is always passed through a synchronizer, and the input state (high or low) must be greater than one TIMCLK clock period for the synchronizer to detect the edge. CCP input edge detection requires at least one TIMCLK cycle to synchronize the edge input. Timing in the first TIMCLK cycle is uncertain because the edge detection cannot be predicted in the first TIMCLK period.
When the capture condition occurs, an additional TIMCLK cycle is required to generate the capture event.