SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519
Devices with multiple flash banks provide a mechanism for swapping the address space of the upper banks with the address space of the lower banks to enable firmware updates where the firmware image itself does not need to have knowledge of the bank it resides in to be able to execute properly on the hardware.
To swap the addresses of the upper flash banks with the addresses of the lower flash banks, set the USEUPPER bit in the FLBANKSWAP register while also writing the KEY value.
Special considerations apply when swapping the flash bank address space. See the nonvolatile memory system chapter of this guide for considerations when using flash bank address swapping.