SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519
For circumstances where accuracy is a key requirement, an external reference can be brought in to the MCU from the VREF+ and VREF- device pins. Only one type of reference (internal or external) can be selected at a time. When supplying the MCU with an external reference, it is recommended to connect a decoupling capacitor on the reference pins with a value based on the voltage source.