To measure the current draw of the MSPM0L1306 MCU using a multimeter, use the 3V3 jumper on the J101 jumper isolation block. The current measured includes the target device, launchpad circuits, and any current drawn through the BoosterPack plug-in module headers.
To measure ultra-low power, follow these steps:
- Remove the 3V3 jumper in the J101 isolation block, and attach an ammeter across this jumper.
- Consider the effect that the
backchannel UART and any circuitry attached to the MSPM0L1306 can have on the
current draw. Consider disconnecting these at the isolation jumper block, or at
least consider the current sinking and sourcing capability in the final
measurement.
- Make sure there are no floating
inputs/outputs (I/Os) on the MSPM0L1306. This causes unnecessary extra current draw.
Every I/O either be driven out or, if the I/O is an input, needs to be pulled or
driven to a high or low level.
- Begin target execution.
- For the most accurate current measurements, place the device in “Free Run” mode and disconnect programming signals between the MSPM0L1306 and the debug portion of the board (header J101).
- Measure the current. Keep in mind
that if the current levels are fluctuating, then getting a stable measurement can be
difficult. Measuring quiescent states is easier.
- Note that the thermistor circuitry on
revision E1 of this board cannot be completely unpowered, and provides additional
current to the measurements unless the thermistor is unpopulated.
EnergyTrace technology can also be used to
compare various current profiles and better optimize your energy performance.