SLAU869E October 2022 – January 2024
The LaunchPad development kit adheres to the 40-pin LaunchPad development kit pinout standard, where pins are available. A standard was created to aid compatibility between LaunchPad development kits and BoosterPack plug-in modules across the TI ecosystem.
While most BoosterPack plug-in modules are compliant with the standard, some are not. The MSPM0L1306 LaunchPad development kit is not compatible with all 40-pin BoosterPack plug-in modules due to the fact that the MSPM0L1306 device does not have enough pins to fill the standard. If the reseller or owner of the BoosterPack plug-in module does not explicitly indicate compatibility with the MSPM0L1306 LaunchPad development kit, then compare the schematic of the candidate BoosterPack plug-in module with the LaunchPad development kit to verify compatibility. Keep in mind that sometimes conflicts can be resolved by changing the MSPM0L1306 device pin function configuration in software.