SLAU869E October 2022 – January 2024
The internal SYSOSC is 32MHz as default at the accuracy of 2.5%. To achieve higher accuracy, a 0.1% 100kΩ resistor is connected to the ROSC pin, PA2. If higher accuracy is not needed, then resistor R6 can be depopulated, and pin PA2 used for the other functions. The MCLK is sourced by 32MHz SYSOSC at default. CPUCLK is sourced directly from MCLK in RUN mode and disabled in other modes. The low-power clock (ULPCLK) can be sourced by MCLK and active in RUN and SLEEP mode by configuration. For more clock tree details see Section 2.3 Clock Module (CKM) of the MSPM0 L-Series 32MHz Microcontrollers Technical Reference Manual.