SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1
Flow control can be accomplished by hardware and the following sections describe the implementation method.
In UART mode (CTL0.MODE set to 0), hardware flow control between two devices is accomplished by connecting the RTS output to the CTS input on the receiving device, and connecting the RTS output on the receiving device to the CTS input. The RTS output signal is low active, the CTS input expects a low signal on a send request as shown in Figure 11-9.
The CTS input controls the transmitter, the Device 0 and Device 1 transmitter can only transmit data when their CTS input is asserted low. When RTS flow control is enabled, the RTS output signal indicates the state of the receive FIFO. For example, the CTS of the Device 1 remains asserted low until the preprogrammed RX FIFO level of Device 0 is reached, indicating that the receive FIFO of Device 0 has no space to store additional characters.
The CTSEN and RTSEN bits in the UART.CTL0 register specify the flow control mode as shown in Table 11-3.
CTSEN | RTSEN | Description |
---|---|---|
1 | 1 | RTS and CTS flow control enabled |
1 | 0 | Only CTS flow control enabled |
0 | 1 | Only RTS flow control enabled |
0 | 0 | Both RTS and CTS flow control disabled |
When RTSEN is set to 1, the value of the CTL0.RTS bit is ignored and the RTS output signal is generated by the hardware trigger levels as described below. When RTSEN bit is cleared, the RTS signal output is controlled by the CTL0.RTS bit for SW control.
RTS flow control:
The RTS flow control logic is linked to the programmable receive FIFO watermark levels, it can be configured using UARTx.IFLS register. When RTS flow control is enabled, the RTS is asserted (low) until the receive FIFO is filled up to the watermark level. When the receive FIFO watermark level is reached, the RTS signal is de-asserted (high), indicating that there is no more room to receive any more data. The transmission of data is expected to cease after the current character has been transmitted. The RTS signal is reasserted (low) when data has been read out of the receive FIFO so that it is filled to less than the watermark level. If RTS flow control is disabled and the UART is still enabled, then data is received until the receive FIFO is full, or no more data is transmitted to it.
As the RTS signal is de-asserted when the FIFO watermark level is reached by putting the last received character into the FIFO. This means on a back to back transmit another character transfer could already been started by the sender. Therefore, in such cases the watermark level should be set to one level lower to ensure all data can be received and put into the FIFO.
CTS flow control:
If CTS flow control is enabled, then the transmitter checks the CTS signal before transmitting the next byte. If the CTS signal is asserted (low), it transmits the byte otherwise transmission does not occur. The data continues to be transmitted while CTS is asserted (low), and the transmit FIFO is not empty. If the transmit FIFO is empty and the CTS signal is asserted (low) no data is transmitted. If the CTS signal is de-asserted (high) and CTS flow control is enabled, then the current character transmission is completed before stopping. If CTS flow control is disabled and the UART is enabled, then the data continues to be transmitted until the transmit FIFO is empty.