SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1104 , MSPM0C1104-Q1
The event manager transfers digital events from one entity (for example, a peripheral) to another (for example, a second peripheral, the DMA, or the CPU). The event manager implements event transfer through a defined set of event publishers (generators) and subscribers (receivers) which are interconnected through an event fabric containing a combination of fixed (static) and programmable routes.
Events which are transferred by the event manager include:
In addition to providing the event transfer logic, the event manager also interfaces with the power management and clock unit (PMCU) if an event requires the power and/or clock configuration of the device to change to handle the event properly. For example, if a peripheral asserts an event that targets the DMA, and the device is in a STOP or STANDBY operating mode (DMA is disabled), the event manager will handshake with the PMCU to suspend the low power operating mode state temporarily and enable the DMA such that the DMA transfer can be processed.
The event manager configuration is device dependent, as different devices support different peripherals. See the device-specific data sheet for information on the device-specific event implementation.