SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1104
Software can generate a software POR, a software BOOTRST, a software SYSRST with bootstrap loader (BSL) entry, or a software SYSRST by issuing the appropriate command to SYSCTL. To issue a reset, first select the desired reset level in the RESETLEVEL register in SYSCTL. Then set the GO bit in the RESETCMD register along with the KEY value.
LEVEL | Action |
---|---|
0x0 | Software SYSRST |
0x1 | Software BOOTRST |
0x2 | Software SYSRST with BSL entry |
0x3 | Software POR |
A CPU-only reset (CPURST) which does not reset the peripherals can also be triggered in software within the Cortex-M0+ CPU by setting the SYSRESETREQ bit in the AIRCR local CPU register. See the CPU Sub System chapter for more information.
The software-triggered BSL entry (RESETLEVEL 0x02) is a special case of the SYSRST which provides a mechanism for the application software to start the ROM bootstrap loader (BSL). It is not possible to jump to the bootloader code directly during normal software execution in RUN mode. When application software commands a software-triggered BSL entry (RESETLEVEL 0x02), a SYSRST is generated first, followed by execution of the boot configuration routine (for authentication), after which the BSL is started (if the device security policy has the BSL configured to be enabled). Once the BSL has completed execution, a second SYSRST is issued and the BCR will execute. When the BCR completes, a final SYSTRST is asserted to return control of the system back to the application software. Any system configuration which is not reset by a SYSRST will be maintained through this entire process.