SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1104
The ADC is configured with user software. The following sections describe the setup and operation of the ADC.
On devices which run MCLK and ULPCLK at the same frequency, there is not a performance benefit to accessing the ADC MEMRES registers through the aliased region. On device configurations where MCLK is greater than ULPCLK, the aliased region is recommended to be used. However, application software can use the aliased region on all devices for MEMRES access to keep the software implementation consistent.