SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1104
The dynamic write protection scheme is intended to be configured at runtime by software. This scheme provides a simple way for application software to specify sectors to protect from modification by any program or erase operations that are issued with the flash controller. Unlike the static write protection mechanism, the dynamic mechanism is not lockable and thus does not provide any level of data security.
There are two primary uses for dynamic write protection. First, it provides an extra level of robustness against unintentional program or erase of specified sectors in applications that involve in-system programming for either firmware updates or EEPROM emulation. Second, it provides a way to simplify a situation where a bank erase is desired but a small number of sectors should not be erased when a bank erase command is issued. One example would be an application running on a single-bank device in which most of the MAIN region sectors are used to store the executable image, but a few sectors are used to store device-specific data that should not be erased during a firmware update. In that case, the sectors containing the device-specific data can be protected with dynamic write protection, and a bank erase command can be issued to erase all other sectors. This has the benefit that the majority of the MAIN region can be erased with a single command (a bank erase) rather than individual sector-by-sector commands, which would have a longer overall erase time and use more energy.
The dynamic write protection scheme is configured by setting up the CMDWEPROTx registers in the flash controller. The CMDWEPROTx registers cover one flash bank at a time. This means that these registers must be configured with knowledge of which flash bank an attempted program or erase operation will be applied to. Note that the CMDWEPROTx registers are reset to a protected state at the end of all program and erase operations. These registers must be re-configured by software before a new operation is initiated.