SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1
The WWDT operating mode (watchdog mode or interval timer mode) is selected by the MODE bit in the WWDTCTL0 register. Watchdog mode is the default mode (MODE cleared). Setting the MODE bit configures the WWDT for interval mode.
When the WWDT is in watchdog mode, the WWDT counter must be restarted within the open window period by writing the RESTART value (0x000000A7) to the WWDTCNTRST register. After a reset or restart, the WWDT counter will restart from zero. A failure to restart the WWDT within the open window or an attempt to restart the WWDT counter during the closed window will generate a WWDT violation to SYSCTL. Writing any value other than the RESTART value to the WWDTCNTRST register also generates a WWDT violation.
When the WWDT is in interval mode, the timer acts as an interval timer, generating WWDT interrupts to the CPU as specified by the WWDT period. As soon as the WWDT is enabled in interval mode, the WWDT interval timer interrupt will be asserted after the expiration of the timer. It is not necessary to restart the WWDT in interval timer mode.