SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1
Certain applications need to place read-only data into SRAM. This can occur if code is placed into SRAM (for zero wait state execution) or if critical lookup tables are placed in SRAM (for zero wait state reads). In these cases, especially when code is to be executed from the SRAM, it is desirable to prevent unintentional writes to SRAM addresses that can corrupt executable code in the event of a buffer overrun or a stack overflow. Likewise, it is desirable to prevent execution from nonwrite-protected SRAM addresses. To improve robustness of data in stored in SRAM, SYSCTL provides a write-exclusive-execute boundary mechanism.
To use this feature, first load the read-only data into the desired SRAM address, then configure the SRAM address range to be write protected. SRAM contents which are to be read-execute (no writes) should be placed into the upper portion of SRAM. SRAM contents which are to be read-write (no execute) should be placed into the lower portion of the SRAM. Then, the SRAMBOUNDARY register may be written with the desired boundary to partition the SRAM into two regions, with the lower region being RW and the upper region being RX.