SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1104
The BCR configuration data for TI factory trim in the NONMAIN memory includes a CRC16 value corresponding to the CRC16 digest of the respective structure. During the device boot process, the BCR will compute the CRC digest of the data structures and compare it with the stored CRC values before the data contained within the structures is trusted for use.
Ifthe TI factory trim fails its CRC check during boot, a catastrophic boot error will also result with the following limitations: