SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1104
The WWDT module provides one interrupt source which can be configured to source a CPU interrupt event. The WWDT interrupt conditions are given in Table 17-198.
Index (IIDX) | Name | Description |
---|---|---|
0 | INTTIM | Indicates that the WWDT interval timer period has expired |
The CPU interrupt event configuration is managed with the CPU_INT event management registers. See Section 6.2.5 for guidance on configuring the Event registers for CPU interrupts.