SLAU900 November 2023
Make sure that the AFE532A3WEVM is not connected to the computer during the software installation.
The AFE532A3WEVM software can be downloaded from the device product folders or AFE532A3WEVM tool folder. After the software is downloaded, navigate to the download folder, and run the SMART-DAC-EVM-GUI installer executable.
When the AFE532A3WEVM software is launched, an installation dialog window opens and prompts the user to select an installation directory. Figure 4-1 shows that the software path defaults to C:\Program Files (x86)\Texas Instruments\SMART-DAC-EVM-GUI.
The software installation also installs the FTDI USB drivers, and automatically copies the required LabVIEW™ software files and drivers to the computer. The FTDI USB drivers install in a second executable. Figure 4-2 shows the window that is automatically launched after the software installation is complete.