SLAU900 November 2023
The AFE532A3WEVM GUI incorporates interactive functions that help configure an individual AFEx32A3W device using I2C or SPI communication. These functions are built into several GUI pages, as shown in the following subsections. The menu bar on the far left of the GUI allows the user to switch between pages. The menu bar displays the High Level Configuration page, with the Basic DAC subpage, and the Low Level Configuration page.
Before using the GUI, see the respective device data sheet for detailed AFEx32A3W programming instructions.