SLAU902A September 2023 – January 2024
The TAx5x12 EVM GUI is an application that installs into the PPC3 framework. PPC3 must be installed prior to downloading the TAx5x12 EVM GUI. Click here to download the PPC3 and request access. If the PPC3 is already installed, then proceed to Section 3.3. Figure 3-1 shows the setup directory for the PPC3 installation.
Open the PPC3 installer and follow the instructions in the setup wizard.