SLAU902A September 2023 – January 2024
The GPIOs function and interrupt behavior, as shown in figure below, can be configured in this tab. There is 1 General Purpose Input (GPI1), 1 General Purpose Output (GPO1) and 2 General Purpose Input Output (GPIO1 and GPIO2) in the TAx5x12 devices. These general purpose input/output drivers also provide several multiplexing functions and the selection can be configured in this tab as well.