SLAU903 October 2023
As shown in the figure below, the GPIO function and interrupt behavior can be configured in this tab. There is 1 General Purpose Input Output (GPIO1) in the TAx5x1x-Q1 devices. These general purpose input/output drivers also provide several multiplexing functions, and the selection can also be configured in this tab..