SLAU905A August 2023 – November 2023 DAC81401
This section provides the procedure for EVM software installation.
The EVM software is compatible with the Windows® 10 operating system. Before installing the software, make sure that the DAC80401EVM is not connected to the local machine.
Download the latest version of the EVM graphical user interface (GUI) installer from the Order and start development subsection of the DAC81401EVM tool folder on TI.com. Run the GUI installer to install the DAC81401EVM GUI software on your local machine.
When the DAC804xxEVM GUI is launched, an installation dialog window opens and prompts the user to select an installation directory. If left unchanged, Figure 2-1 shows that the software location defaults to C:\Program Files (x86)\Texas Instruments\DAC814xxEVM.
The EVM software also installs the Future Technology Devices International Limited (FTDI) USB drivers using a separate executable file. Figure 2-2 shows the FTDI USB drivers installation window that is automatically launched after the DAC814xxEVM software installation is complete.