SLAU909A September   2023  – December 2023 ULC1001

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. General Texas Instruments High Voltage Evaluation (TI HV EVM) User Safety Guidelines
  5. Introduction
  6. Hardware Overview
  7. What's in the Box
  8. Getting Started
  9. LED Status Indicator
  10. Schematics
  11. Layout
  12. Dimensions
  13. 10Revision History

What's in the Box

The Camera Module contains three circuit boards. From front to back, these boards are the camera module, the driver board, and a connector board for passing all signals. The device has two ports on the back: one Micro-USB for the camera and one USB-C for passing power and Inter-Integrated Circuit (I2C) communication to the driver board. The Micro-USB can optionally be connected to a Windows 10 PC. ULC-HPB-DEMO can run on the native Windows Camera app without downloading and installing additional software. The USB-C needs to be connected to the Switch Box.

GUID-20230728-SS0I-JDBN-QKXJ-NR4SLPSRJSWZ-low.png Figure 4-1 Camera Module

The switch box controls the ultrasonic lens cleaning in the camera module. The barrel jack plugs into the supplied switching adapter. The USB-C output plugs into the camera module.

WARNING: GUID-7CDBB8AD-0357-43FF-82A1-14CF96AE0E4B-low.gif All high voltage is enclosed in the camera module.
GUID-20230728-SS0I-Q24X-5JRL-KB9J43GT5NFB-low.png Figure 4-2 Switch Box

The additional hardware includes:

  1. Switching power supply, 36W power adapter accepts 110-240 VAC 50/60 Hz
  2. USB-C Cable - connects the Camera Module and the Switch Box
  3. Barrel jack adapter for the power supply
  4. USB-A to Micro USB-B Cable
  5. Empty spray bottle
GUID-20230823-SS0I-W6VF-NND3-V11JNLRCNF6N-low.png Figure 4-3 Additional Hardware