SLAU913 august 2023 AFE539A4
This section describes the overall system setup for the EVM. A computer runs the software that provides an interface to the AFE539A4EVM through the on-board controller.
The USB connection generates 5-V of power for use as the DAC supply voltage (VDD). The on-board controller supplies 3.3-V of power for the input/output (IO) signals from the controller. These IO signals are level translated to the VDD voltage of the DAC. Figure 3-2 displays the system hardware setup.