The ULC1001-DRV2911EVM image is shown in ULC1001-DRV2911EVM. The entire EVM, LCS, and USB2ANY setup is shown in Figure 3-1. Follow these instructions to setup the system.
- Flip PWR switch off (off = O).
- With the power supply unplugged or off, connect to J3 or J4. Input 9-16V, 8A. The 8A current is based on load requirements.
- Make sure the LCS or load is discharged and plug the LCS cable into the J2 terminal block. Output, 0-250 Vp, 3.5A, 10-400 kHz.
- Connect the 10-pin I2C ribbon cable from the ULC1001-DRV2911 EVM to the USB2ANY using J1.
- Connect the mini USB cable from the USB2ANY into the computer.
- Verify all safety procedures are followed before powering on the device (for example, personal protective equipment or a protective enclosure for the EVM setup).
- Turn on the power supply.
- Flip the Power Switch switch to the on position (on = I).
- Download and install the ULC1001 GUI available on TI mySecureSoftware.
CAUTION:  |
Do not leave EVM powered when unattended. |