SLAU916 May 2024
The DAC80516EVM is connected to the computer through the on-board FT4232 digital controller using the USB cable that is supplied with the EVM. The evaluation board features connectors and test points for all communication lines, DAC outputs, digital pins, and supplies. Figure 3-1 shows a block diagram of the DAC80516EVM.
The USB connection provides the 5V supply to the EVM. Voltage regulators generate 3.3V and 1.8V from the USB 5V supply. These 3.3V and 1.8V supplies are used to power the FT4232 controller.
The DAC80516 AVDD supply can use the on-board 5V or 3.3V supplies depending on the jumper J6 setting. By default, AVDD is connected to the on-board 5V supply. Alternatively, AVDD can be supplied externally through banana jack J4. Remove the jumper connector on J6 before connecting external supplies to AVDD.
The DAC80516 VIO supply can use the on-board 1.8V or use the same voltage as AVDD depending on the jumper J5 setting. By default, VIO is connected to AVDD. Alternatively, VIO can be supplied externally through banana jack J8. Remove the jumper connector on J5 before connecting external supplies to VIO.
The device reference voltage can be supplied via an on-board 2.5V voltage regulator by shorting jumper J12, or from an external supply with SMA J10. Make sure that the DAC80516 internal reference is powered off before connecting any other voltage supply to the REF pin.
Each of the DAC outputs have optional capacitative and resistive loads that are not populated by default. In addition, C36 is a dedicated capacitor footprint that is isolated from the ground and power planes of the EVM. This capacitor can be used for precise glitch measurements.