SLAU927A March 2024 – June 2024 MSPM0G3507
For applications that require stopping the motor quickly, configure Motor stop options [MTR_STOP] to either Low side braking:
Step 1: Configure Motor stop options [MTR_STOP] to Low side braking.
Step 2: Select Speed threshold for BRAKE pin and Motor STOP options. Setting speed threshold to higher speed can result in FETs carrying large current. Setting speed threshold to lower speed results in increase in the stop time of the motor. Recommended to start with 50% of the maximum speed, If the motor phase current exceeds the FET maximum current rating, then decrease the threshold. If the stop time is too high, then recommended to increase the threshold without hitting the maximum current limit.