Follow the steps below when connecting an MSPM0 LaunchPad to a DRV83xx EVM:
- Connect the three motor phase terminals to the driver board (phases A, B, and C). If the motor has a center tap connection or wires for Hall-effect sensors, leave these wires unconnected.
- Make the inter-device connections from the MSPM0 LaunchPad kit to the DRV83xx EVM by mating the EVM to the LaunchPad kit or using jumper wires as shown in Figure 2-4. See Section 2.1.1 for hardware user guide connection details.
Note: If using the GUI to communicate to the MSPM0 device using USB to backchannel UART, connect the backchannel UART connections to UART3_TX and UART3_RX as shown in
Figure 2-5.
- Connect a micro-USB cable from the MSPM0 LaunchPad kit to the PC.
- Remove GND and 3V3 isolation jumpers on the bridge if desired to isolate the PC from the motor system. If this step is done, 3V3 must be provided externally or from the DRV83xx EVM board, if available.
- Supply a voltage compliant with the Power Supply Voltage (VM) range. See the board-specific user's guide or DRV-specific data sheet for recommended voltage range.