SLAU927B June 2024 – November 2024 MSPM0G3507
FOC Algorithm enables user to brake the motor under various scenarios. Brake state can be configured to either low side braking ( Low-Side Braking) or align brake ( Align Braking) through BRAKE_PIN_MODE. FOC Algorithm decreases output speed to value defined by BRAKE_SPEED_THRESHOLD before entering brake state. As long as BRAKE is driven 'High', motor stays in brake state. Brake functionality can be achieved the following way:
User can configure the BRAKE_INPUT in PIN_CONFIG register to apply the brakes using register settings as below.