VBAT supply to TAS2320 is powered by 5V connected to VBAT barrel jack J21.
J5 on the bottom side of the EVM can be used to
select between 2 different sources for VBAT.
- VIN (J21) is selected by default, which is the
barrel jack supplied by 5V.
- VBAT (J30) is an alternative banana jack that can
be used to supply VBAT to TAS2320 - U1 only. Use this for current and efficiency
measurements.
CAUTION: 5V must be connected
to barrel jack J21 even if using J30 for VBAT connection to TAS2320. VIN (J21) is
used to power other things in the EVM.