Hall Invalid fault is triggered if the
FOC application detects an invalid Hall State such as '0' or
'7". This fault is reported through the Fault status Lock
fault.
In case of Hall Invalid fault follow below steps to root cause the issue.
- Make sure the Hall pin connections are pulled up atleast to 3.3v and check the
pin values are toggling as you rotate the motor shaft manually.
- Check the GPIO's connected to the Hall pins are configured appropriately in the
SYCONFIG.
- Check the variation of the GPIO pin values in the register view in CCS debug
window as you manually rotate the shaft.