SLAU948 October 2024 MSPM0G3507
User need to input the Maximum Power Rating of the motor when Closed loop Power Control is required. To determine the Maximum Rated Power of the motor, see the Motor data sheet and compute the product of Rated Motor Voltage in Volts and Rated Motor Current in Amps and feed the value to MOTOR_MAX_POWER in the System parameters.