Advisories that affect the device's operation, function, or parametrics.
✓ The check mark indicates that the issue is present in the specified revision.
Errata Number | Rev E |
---|---|
ADC24 | ✓ |
ADC25 | ✓ |
ADC27 | ✓ |
ADC29 | ✓ |
ADC42 | ✓ |
ADC69 | ✓ |
AES1 | ✓ |
COMP4 | ✓ |
COMP10 | ✓ |
CPU46 | ✓ |
CPU47 | ✓ |
DMA4 | ✓ |
DMA7 | ✓ |
DMA8 | ✓ |
DMA10 | ✓ |
FLASH29 | ✓ |
FLASH31 | ✓ |
FLASH37 | ✓ |
MPY1 | ✓ |
PMAP1 | ✓ |
PMM8 | ✓ |
PMM9 | ✓ |
PMM10 | ✓ |
PMM11 | ✓ |
PMM12 | ✓ |
PMM14 | ✓ |
PMM15 | ✓ |
PMM17 | ✓ |
PMM18 | ✓ |
PMM20 | ✓ |
PORT15 | ✓ |
PORT16 | ✓ |
PORT17 | ✓ |
PORT19 | ✓ |
PORT21 | ✓ |
RF1A1 | ✓ |
RF1A2 | ✓ |
RF1A3 | ✓ |
RF1A5 | ✓ |
RF1A6 | ✓ |
RF1A8 | ✓ |
RTC3 | ✓ |
RTC6 | ✓ |
SYS16 | ✓ |
TAB23 | ✓ |
UCS6 | ✓ |
UCS7 | ✓ |
UCS9 | ✓ |
UCS10 | ✓ |
UCS11 | ✓ |
USCI26 | ✓ |
USCI30 | ✓ |
USCI31 | ✓ |
USCI34 | ✓ |
USCI35 | ✓ |
USCI39 | ✓ |
USCI40 | ✓ |
WDG4 | ✓ |
Advisories that are resolved by compiler workaround. Refer to each advisory for the IDE and compiler versions with a workaround.
✓ The check mark indicates that the issue is present in the specified revision.
Errata Number | Rev E |
---|---|
CPU18 | ✓ |
CPU20 | ✓ |
CPU21 | ✓ |
CPU22 | ✓ |
CPU23 | ✓ |
CPU24 | ✓ |
CPU25 | ✓ |
CPU26 | ✓ |
CPU27 | ✓ |
CPU28 | ✓ |
CPU29 | ✓ |
CPU30 | ✓ |
CPU31 | ✓ |
CPU32 | ✓ |
CPU33 | ✓ |
CPU34 | ✓ |
CPU35 | ✓ |
CPU39 | ✓ |
CPU40 | ✓ |
Refer to the following MSP430 compiler documentation for more details about the CPU bugs workarounds.
TI MSP430 Compiler Tools (Code Composer Studio IDE)
MSP430 GNU Compiler (MSP430-GCC)
IAR Embedded Workbench
The revision of the device can be identified by the revision letter on the Package Markings or by the HW_ID located inside the TLV structure of the device.