Advisories that affect the device's operation, function, or parametrics.
✓ The check mark indicates that the issue is present in the specified revision.
Errata Number | Rev H | Rev F | Rev E |
---|---|---|---|
ADC25 | ✓ | ✓ | ✓ |
BCL12 | ✓ | ✓ | ✓ |
BCL13 | ✓ | ||
BCL15 | ✓ | ✓ | ✓ |
DAC4 | ✓ | ✓ | ✓ |
DMA3 | ✓ | ✓ | ✓ |
DMA4 | ✓ | ✓ | ✓ |
DMA13 | ✓ | ✓ | ✓ |
FLASH19 | ✓ | ✓ | ✓ |
FLASH24 | ✓ | ✓ | ✓ |
FLASH25 | ✓ | ||
FLASH27 | ✓ | ✓ | ✓ |
FLASH36 | ✓ | ✓ | ✓ |
PORT10 | ✓ | ✓ | ✓ |
PORT12 | ✓ | ✓ | ✓ |
TA12 | ✓ | ✓ | ✓ |
TA16 | ✓ | ✓ | ✓ |
TA21 | ✓ | ✓ | ✓ |
TAB22 | ✓ | ✓ | ✓ |
TB2 | ✓ | ✓ | ✓ |
TB16 | ✓ | ✓ | ✓ |
TB24 | ✓ | ✓ | ✓ |
USCI20 | ✓ | ✓ | ✓ |
USCI21 | ✓ | ✓ | ✓ |
USCI22 | ✓ | ✓ | ✓ |
USCI23 | ✓ | ✓ | ✓ |
USCI24 | ✓ | ✓ | ✓ |
USCI25 | ✓ | ✓ | ✓ |
USCI26 | ✓ | ✓ | ✓ |
USCI27 | ✓ | ✓ | ✓ |
USCI30 | ✓ | ✓ | ✓ |
USCI34 | ✓ | ✓ | ✓ |
USCI35 | ✓ | ✓ | ✓ |
USCI40 | ✓ | ✓ | ✓ |
XOSC5 | ✓ | ✓ | ✓ |
XOSC8 | ✓ | ✓ |
Advisories that affect factory-programmed software.
✓ The check mark indicates that the issue is present in the specified revision.
The device does not have any errata for this category.