SLAZ196I October 2012 – May 2021 MSP430F423
ESP Module
Functional
In two current mode, CAPIND detection works on current channel 1 only
When using the ESP430 module in the two current mode, CAPIND detection works on current channel 1 only and does not work when using current channel 2. This could deliver wrong values if the current in channel 1 is near or equal 0.
None