SLAZ548T July 2013 – May 2021 MSP430F5249
PORT Module
Functional
P4.6 is not set to input floating if device is in RESET state
P4.6 is driven active low while the MSP430 device is held in a reset state. This can influence components connected externally that are expecting the pin to act as a floating input during MSP430 reset.
Use any other GPIO if input floating state is required while the device is in a reset state.