SLAZ666T April 2015 – May 2021 MSP430FR59221
ADC Module
Software in ROM
Invalid ADC12 temperature sensor calibration data
The ADC12 reference temperature sensor calibration data stored in the TLV data structure (0x1A1A - 0x1A25) can be incorrect depending on the production lot trace code.
As a result the temperature measurement when using these data can be wrong.
Devices with lot trace code > 88XXXXX are not affected by this issue.
Record the calibration data by taking ADC measurements of the temperature sensor at 30C and 85C for the required reference voltage. The calibration data in the TLV section (0x1A1A - 0x1A25) can't be overwritten but the new calibration data can be stored in user FRAM or info memory for further temperature calculations.