SLIA097 March 2022 DRV5011 , DRV5011 , DRV5012 , DRV5012 , DRV5013 , DRV5013 , DRV5015 , DRV5015 , DRV5021 , DRV5021 , DRV5023 , DRV5023 , DRV5032 , DRV5032 , DRV5033 , DRV5033 , TMAG5110 , TMAG5110 , TMAG5111 , TMAG5111 , TMAG5123 , TMAG5123 , TMAG5231 , TMAG5231 , TMAG5328 , TMAG5328
Hall-effect sensor bandwidth is specified as a digital characteristic, differing from analog bandwidth in devices like operational amplifiers. Bandwidth determines the maximum frequency capable of being sensed by a Hall-effect sensor. It is necessary to consider the total number of magnetic poles present in the flow meter to verify if the maximum rotational speed of the impeller is less than the bandwidth of the device. For example, a flow meter using a high bandwidth DRV5013 Hall-effect latch (30 kHz) and ring magnet with 32 poles (16 North oriented, 16 South oriented) has a maximum typical theoretical sensing speed of 1875 rotations per second. Using the calculated maximum rotational sensing speed to verify the maximum flow rate does not cause the mechanical assembly to exceed the sensing capability for the Hall-effect device.